FAQ

Engineered solutions pressure

Can each pressure transmitter measure any medium?

No, the materials stated in the data sheet are to be checked by the customer for resistance.

What solutions are there against pressure spikes?

For this, we recommend a process connection with a reduced pressure port of 0.6 mm or 0.3 mm.

What is the overpressure limit?

Pressures up to the overpressure limit will not cause any permanent damage to the measuring instrument, however, the error limits specified in the data sheet could be exceeded.

At what pressure could the pressure measuring instrument be destroyed?

Pressure values above the overpressure limit can lead to irreversible damage of the measuring instrument. It does not matter whether this pressure is present constantly or only for a short period of time. In either case, the complete destruction of the parts exposed to the pressure and the sudden escape of the pressure medium can be expected.