Thermometers with switch contacts

Wherever the process temperature has to be indicated locally and, at the same time, limit values must be monitored, thermometers with switch contacts find their application. The switch contacts make or break the circuit dependent upon the pointer position of the indicating measuring instrument. If the reading is significantly above or below a set value, they trigger an alarm, hence also the term “alarm contact”. The instruments are also suitable for starting, stopping or switching processes.

Sales contact Questions? Find a contact in your vicinity.


FAQ

Can mechanical dial thermometers with a CE marking be placed on the market?

With CE marking, the manufacturer, the company or person placing the product on the market or the EU authorised representative declares that the product complies with all relevant European guidelines.
Since there is no binding instruction (directive) for mecha ... More

What is a change-over contact?

When the set point is exceeded, simultaneously one circuit is opened (NC) and one circuit is closed (NO). Changeover contacts are denoted by the number 3 (SPDT).

Wish list - Documents (0)

There are currently no documents on your wish list. You can add any document from the download area to your wish list. To do this, select the desired language using the flag symbol.

The maximum number of 20 entries was reached.

To receive your download link via e-mail, enter your address here:

The e-mail address is invalid.