Multipoint thermometers

Multipoint sensor assemblies are used in various applications in the refining and petrochemical industry. WIKA is a world leader in flexible multipoint sensor thermometry and the preferred solution of many major companies and licensors. Our preferred advanced multipoint solutions, including FLEX-R® and FLEX-O®, are recognised as leading technologies in the industry. Additional multipoint products for global market requirements include traditional multipoint designs such as pipewells, T-bar, spring-loaded, bimetallic spring, and heat transfer block. Innovative mini-multipoint solutions where point density and thermocouple size matter include both stuffed and drawn assemblies to solve challenging applications.

Sales contact Questions? Find a contact in your vicinity.


FAQ

Does the FLEX-R® (model TC96-R) include a secondary seal?

Yes, FLEX-R® assemblies can have a primary seal weld and a secondary seal weld from the thermocouple to the flange assembly at the face of the flange, not on a single disk, and again after the secondary containment chamber.

What is a secondary containment chamber?

The secondary containment chamber is a sealed chamber (neck tube) between the primary seal weld and secondary seal weld that contains an instrument connection. In the event of a primary weld failure, the secondary containment chamber would pressure up to operating ... More

Wish list - Documents (0)

There are currently no documents on your wish list. You can add any document from the download area to your wish list. To do this, select the desired language using the flag symbol.

The maximum number of 20 entries was reached.

To receive your download link via e-mail, enter your address here:

The e-mail address is invalid.