Temperature switches

Temperature switches are used in a variety of industrial and technical processes. If a preset temperature is reached, then the temperature switch opens or closes a corresponding switch contact. Depending on the requirements, mechanical or electronic switches can be used. In WIKA's broad product range, you will find the right temperature switch for every application.

Sales contact Questions? Find a contact in your vicinity.


FAQ

What minimum insertion lengths are recommended, as a rough guide, for protection tubes in order to minimise the heat dissipation error?

for gaseous media: 15 ... 20 x protection tube diameter
for liquid media: 5 ... 10 x protection tube diameter
for solid media: 3 ... 5 x protection tube diameter
(these standard values are only valid for static mediaThe gap between the protection tub ... More

What is the repeatability with mechanical pressure or temperature switches?

The repeatability is one of the most important performance characteristics for pressure or temperature switches. It describes the maximum deviation between the switch points when repeatedly approaching the same pressure or temperature value. This value indicates ho ... More

Wish list - Documents (0)

There are currently no documents on your wish list. You can add any document from the download area to your wish list. To do this, select the desired language using the flag symbol.

The maximum number of 20 entries was reached.

To receive your download link via e-mail, enter your address here:

The e-mail address is invalid.