Our website uses cookies. By continuing to use it, you agree to their use.
Solutions for pressure, temperature, force and level measurement, flow measurement, calibration and SF6 gas solutions from WIKA are an integral component of our customers' business processes.
This is why we consider ourselves to be not just suppliers of measurement components but rather more a competent partner that offers comprehensive solutions in close co-operation with our customers – customised and precisely designed products for the exact requirement.
Water jet cutting
Water jet cutting is used in many sectors of industry and the materials to be processed are almost unlimited: Metal, stone, glass, composite materials or even food. Cutting with water pressure offers advantages over plasma cutting or laser cutting.
In addition, there are no tooling costs for water jet cutting, in contrast to machining with a punch. In abrasive water jet cutting, an abrasive is added to the coherent high-pressure water jet. Modern water jet cutting systems work with up to 6,000 bar water pressure and the jet leaves the cutting nozzle at 3 times the speed of sound. To protect the pump from cavitation and dry running, an adequate water flow is required. WIKA has the right switches both for monitoring the inlet pressure and also for temperature monitoring.
Page
of 4