Temperature switches

Temperature switches are used in a variety of industrial and technical processes. If a preset temperature is reached, then the temperature switch opens or closes a corresponding switch contact. Depending on the requirements, mechanical or electronic switches can be used. In WIKA's broad product range, you will find the right temperature switch for every application.

Sales contact Questions? Find a contact in your vicinity.


FAQ

Why has there been, for some time, a separation between the accuracy classes for "wire-wound resistance" and "film resistance" Pt100 measuring resistors?

In the past, no distinction had been made between the two basic types of measuring resistor and their temperature limits.  Practice, however, showed that film resistors (thin-film/chipset resistors) have a (not insignificant) deviation form the characteristic. ... More

What does one understand by the accuracy of mechanical pressure or temperature switches?

With the accuracy, one refers to the deviation between the set point and the actual value of the switch point. The “accuracy” is only used very rarely with mechanical pressure or temperature switches, because the set point is often set by the custome ... More

Wish list - Documents (0)

There are currently no documents on your wish list. You can add any document from the download area to your wish list. To do this, select the desired language using the flag symbol.

The maximum number of 20 entries was reached.

To receive your download link via e-mail, enter your address here:

The e-mail address is invalid.