Contact pressure gauges

WIKA contact pressure gauges: Switching and indicating with a single instrument

Wherever the process pressure has to be indicated locally and, at the same time, limit values must be monitored, contact pressure gauges find their application. The switch contacts make or break the circuit dependent upon the pointer position of the indicating measuring instrument. If the reading is significantly above or below a set value, they trigger an alarm, hence also the term “alarm contact”. Contact pressure gauges are also suitable for starting, stopping or switching processes.

Calibration services

Entrust the calibration and maintenance of your measuring instruments to a competent partner.

Details
Sales contact Questions? Find a contact in your vicinity.


FAQ

How low is the temperature of the medium which is stored inside the cryogenic vessel when it reaches the pressure gauge?

A Cryo gas is a gas which is gaseous at ambient temperature and pressure and becomes liquid because of cooling and compression. Due to cooling and compression the volume of the gas can be reduced and thus it’s possible to store a huge quantity inside a ves ... More

When should a restrictor be used?

For pressure spikes or sudden pressure loading and unloading.

Wish list - Documents (0)

There are currently no documents on your wish list. You can add any document from the download area to your wish list. To do this, select the desired language using the flag symbol.

The maximum number of 20 entries was reached.

To receive your download link via e-mail, enter your address here:

The e-mail address is invalid.