Our website uses cookies. By continuing to use it, you agree to their use.
Contact us for more information.
Temperature calibration can be accomplished in a variety of ways and with various degrees of accuracy. As with any calibration, a standard must be used. The standards used in temperature calibration can come in different forms but must be certified with an accuracy that is traceable to a national standard. In industrial applications temperature calibration usually involves thermistors, thermocouples or Platinum resistance thermometers (PRTs), also called resistance temperature devices (RTDs). These are devices used to accurately measure temperature. Readings from these devices can be compared with less accurate field temperature sensors and used to evaluate the viability of those devices or to perform a temperature calibration.
The temperature calibration usually consists of an 'as found' check to make sure the temperature probe is within the calibration tolerances. If a probe is found to be out of tolerance it is typically replaced with a new probe that is in tolerance. Alternatively, offsets to correct the out of tolerance condition can be made directly to the electronic transmitter connected to the temperature sensor. The cost of the temperature probe verses the cost of adjusting the transmitter should be considered in determining the most feasible method. In either case, the temperature calibration should be conducted over the specified range of the sensor or its range of application.
Simply reading the temperature from a temperature sensor using a RTD or a thermocouple indicator and then checking the in line field indicator to see if the reading are the same is not a temperature calibration. Simulating that temperature output to a read out device is a good check that the readout is showing the correct reading for a given output for an RTD or Thermocouple, but this also is not a Temperature calibration. A temperature calibration can only be performed by comparing a known standard, in a stable temperature environment to the probe being tested.
Multi-functional precision thermometer
Reference thermometer
Temperature baths & block calibrator
To perform a temperature calibration one needs a stable and adjustable source of temperature to generate temperatures over the range of the device being calibrated. There are several ways to do this. WIKA calibration baths and dry blocks can provide range of stable temperatures. After a stable temperature is reached, one must have an accurate way to measure that temperature and compare that measurement to the device being tested. WIKA precision thermometers (previously branded ASL) can indicate the temperature from a standard probe then the output from the test probe (immersed in the same temperature bath or dry block) can be compared and recorded in the temperature calibration document. With these Wika Instruments, temperature calibration is possible in ranges from -200 … +1,300 °C (control range -55 … +1,100 °C).
Video
How does a resistance thermometer work? | Resistance thermometers per IEC 60751
Thermocouple basic working principles | How does a thermocouple work?
Calibration Technology
Find the full line of WIKA Temperature instruments at this link.